AXIS#.GEAR.OUT

Description

This parameter is the numerator of the gear ratio for the electronic gearing mode. The gear ratio is used to increase/decrease the slave velocity. The slave velocity can be calculated by the following formula:

Slave velocity = Master velocity * AXIS#.GEAR.OUT/AXIS#.GEAR.IN

Be sure the external master source number of signals per revolution is set correctly. See AXIS#.GEAR.FBSOURCE to determine the gearing master source and verify the feedback resolution for that device.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

-32,768 to +32,767

Default Value

1

Data Type

Integer

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.GEAR.OUT

5006h

04h

Signed16

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5504

1

5504 (0x1580)

AXIS1.GEAR.OUT

Signed16

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.GEAR.OUT

5504

Signed16

Read/Write

-